Technical FAQs

Ask a Question

Does the Powerpact H and J beaker have a true two pole module, or do they use the three pole module?

A true two pole is available for the HD and HG only.

CTA-ID : 2022654
Was this helpful?
What can we do to improve the information ?