Technical FAQs

Ask a Question

What are the dimensions and weight for ATV58HU90M2ZU, ATV58HD12M2ZU, ATV58HD12N4XZU or ATV58HD16N4XZU?

9.06 inches (230 mm) wide
12.80 (325 mm) inches tall
8.27 (210 mm) inches deep
The weight is 26 pounds, 11.9 kg.


CTA-ID : 2022636
Was this helpful?
What can we do to improve the information ?