Technical FAQs

Ask a Question

Does Sq D offer a QO, 200 Amp main breaker load center with feed thru lugs?

Issue:
Product Design

Product Line:
QO Load centers

Environment:
Feed Through lugs

Cause:
application

Resolution:
Yes, there are several QO catalog numbers available with Feed Thru Lugs. See below catalog numbers
1) Can use a QO12436L200TFT with a QOM2200VH MB.
2) Can use a QO12436M200TFT
3) Can use a QO1816M200FTRB


CTA-ID : 2021489
Was this helpful?
What can we do to improve the information ?