Technical FAQs

Ask a Question

What is the maximum ampere rated EZM branch device that is available with EZM metering?

Issue:
Current ampere size of product available.

Product Line:
EZM Metering

Environment:
Maximum Ampere Meter socket.

Cause:
Ampere size of meter socket

Resolution:
The Maximum Ampere rated EZM branch metering device is 400Amp commercial branch unit.


CTA-ID : 2021902
Was this helpful?
What can we do to improve the information ?