Technical FAQs

Ask a Question

Can a DT321 be switched between two loads instead of two sources?

Yes, see wiring diagram in the switch for instructions


CTA-ID : 2021891
Was this helpful?
What can we do to improve the information ?