Technical FAQs

Ask a Question

Is the ATV31 available with bypass?

No, the Altivar 31 is an open type drive designed for panel mounting by the customer. SquareD does not have the ATV31 available as an enclosed package.

The customer certainly can design and build their own bypass circuit to connect to the ATV31. Care should be taken to ensure proper isolation at the drive output power terminals and proper motor overload protection on the bypass circuit.

CTA-ID : 2021453
Was this helpful?
What can we do to improve the information ?