Technical FAQs

Ask a Question

What is the wire range of the lugs and knockout pattern on a busway tap box ending in ETBMB? It is a 3000A tap box.

These End Cable Tap Box has no knockouts. The standard lugs provided have a wire size range from 1/0 to 600 kcmil.

CTA-ID : 2021885
Was this helpful?
What can we do to improve the information ?