Technical FAQs

Ask a Question

What does the ``E`` mean on the end of a part number for a Med.voltage fuse??

The ``E`` that follows the amp rating on the fuse, indicates that it is a ``E`` rated fuse, and that it meets E requirements per ANSI C37.46


CTA-ID : 2021862
Was this helpful?
What can we do to improve the information ?