Technical FAQs

Ask a Question

What can be done when identify an ATV58HC19N4XZU that has an InI fault on power up?

The first thing need to be done is identify the version number of the keypad being used on unit.
As of December 2004, all ATV58HC19N4 size drives need to be ordered with keypad part number VW3A58101V5337.
This keypad is revision 5.3 IE 37 and is compatible with ATV58HC19N4 drives sold in the US.
Other revisions of the Altivar 58 keypad will not operate properly with this drive.
When an order is placed for the ATV58HC19N4XZU, a message appears that indicates special consideration to the keypad part number.


CTA-ID : 2021437
Was this helpful?
What can we do to improve the information ?