Technical FAQs

Ask a Question

How does the QO70AN mount in a load center and is it a 'fork' type neutral lug?

Product Design Features

Product Line:
QO and Homeline load centers


The QO70AN is a 'Fork' type neutral lug that mounts in two of the wire binding holes in a branch neutral bar or PK ground bar and uses the wire binding screws for those holes tighten the lug in place. 

CTA-ID : 2021435
Was this helpful?
What can we do to improve the information ?