Technical FAQs

Ask a Question

What lugs are included in the MMLK600 kit?

The kit includes three double barrel lugs (for both phases and neutral). Each lug will accept (2) #2 - 600 kcmil conductors. This kit also includes lug landing pads (catalog number MMSK2), required for adapting the alternate lugs to the factory supplied lugs mounting pattern. Note: Use two kits for three phase applications.

CTA-ID : 2021427
Was this helpful?
What can we do to improve the information ?