Technical FAQs

Ask a Question

Is the 9007 HA7 lever arm bendable?

Yes it is. So are the 9007 HA5, HA6, HA8, HA9, HA25, HA23, HA20, HA26 and HA21.


CTA-ID : 2021635
Was this helpful?
What can we do to improve the information ?