Technical FAQs

Ask a Question

What is the current draw or consumption of XVP Indicating Banks?

LED units - 24Vac/dc: <60mA; 120-230Vac: <20mA
Steady incandescent bulb 7 W - 24Vac/dc: <300mA; 120-230Vac: 65-35mA
Flashing - 24Vac or 24Vdc: <250mA; 120-230Vac: <30mA
Unit with strobe (on energization) - 24Vdc: 0.3 Joules - 40mA; 120VAC: 0.6 Joules - 20mA; 230Vac: 0.6 Joules - 11mA
Audible sounder units - 24Vdc - 12mA; 120Vac - 15mA; 230Vac - 15mA


CTA-ID : 2021625
Was this helpful?
What can we do to improve the information ?