Technical FAQs

Ask a Question

What are the dimensions for the part number VW3A58407 RFI (EMC) filter for the ATV58?

9.5 inches (240 mm) wide
27.2 inches (690 mm) tall
3.3 inches (85 mm) deep


CTA-ID : 2021419
Was this helpful?
What can we do to improve the information ?