Technical FAQs

Ask a Question

What is the temperature rating of an 8501KPD12?

Operating Temperature Range
KF, KP, KU
AC: 2 pole: -40?C to +55?C (-40?F to +131?F) 3 pole: -40?C to +45?C (-40?F to +113?F)
DC: -40?C to +70?C (-40?F to +158?F)
KL
AC/DC: -45?C to +70?C (-49?F to +158?F)



CTA-ID : 2019853
Was this helpful?
What can we do to improve the information ?