Technical FAQs

Ask a Question

What are the repair parts for the SC8L125F Series M01?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056161350
Meter Cover Mounting Screws - (2) 4020513002K (This kit contains 10 screws, but only two screws required to secure the cover)
Utility Pullbox Cover - 4056172250 (Includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056131452 (Includes hinges)
Load Center Cover Mounting Screws - (4) 2142217101
Dead Front Interior Trim - 4056188201
Dead Front Interior Trim Mounting Screw - 4020513001K (This kit contains 10 screws, but only one screw required to secure the interior trim)
Load Center Interior - 4056164050
Load Center Interior Mounting Screw - (4) 2153217161
Meter Base Assembly - 4056210850 (Includes meter base with the left, load side meter jaw, blade guide and L-shaped connector assembled to the meter base)
Meter Jaw - (3) 4052706950 (OBSOLETE - REPLACED BY 7329794850) (Fourth is included in the Meter Base Assembly, noted above)
Meter Jaw Mounting Bolt - (3) 2271020242 (Fourth is included in the Meter Base Assembly, noted above)
Meter Jaw Mounting Keps Nut - (3) 2342702001 (Fourth is included in the Meter Base Assembly, noted above)
Meter Jaw Blade Guide - (3) 4052761901 (Fourth is included in the Meter Base Assembly, noted above)
Meter Sealing Ring - 2920910001
Line Side Phase Lugs - (2) 4025102450
Line Side Phase Lugs Mounting Bolt - (2) 2271020242
Line Side Phase Lugs Mounting Keps Nut - (2) 2342702001
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE


CTA-ID : 2565
Was this helpful?
What can we do to improve the information ?