Technical FAQs

Ask a Question

Can the QOU single pole Fingersafe Covers be used on 2 and 3 pole QOU`s?

The QOULFSC1 can be used for 10-70amp 1 and 2 pole, or 10-60amp 3 pole QOU breakers. Two covers required per pole.
The QOUHFSC1 can be used for 80-100 amp 1,2, and 70-100 amp 3 pole QOU breakers. Two covers required per pole.


CTA-ID : 2021396
Was this helpful?
What can we do to improve the information ?