Technical FAQs

Ask a Question

Can the LDB12J junction box also be used as a ``cross``?

Yes. The Junction Box includes two closure plates. The box can be used as a ``left`` or ``right`` 90 degree elbow, or a ``tee`` by removing one closure plate, or a ``cross`` by removing both closure plates.


CTA-ID : 2021392
Was this helpful?
What can we do to improve the information ?