Technical FAQs

Ask a Question

What is the speed regulation on the ATV31 unit?

The speed regulation is the same as with the ATV58 in open loop. It is +/- 1%.


CTA-ID : 2021012
Was this helpful?
What can we do to improve the information ?