Technical FAQs

Ask a Question

What is the standard braking torque characteristics for the Altivar 58 type drive?

30% of nominal motor torque without dynamic braking (typical value).
Up to 150% with the dynamic braking option (for constant torque ratings).


CTA-ID : 2020933
Was this helpful?
What can we do to improve the information ?