Technical FAQs

Ask a Question

Can the ATV66 operate off of Ethernet communication with the addition of a card?

There was no direct option card that was available to allow for Ethernet communication on the ATV66.
To operate Ethernet would need to have Modbus option card part number VW3A66301U and an Ethernet/Modbus bridge part number 174CEV30020.
Keep in mind that the Altivar 66 is now an obsolete product. Therefore, it is recommended to use current products when possible.


CTA-ID : 2020860
Was this helpful?
What can we do to improve the information ?