Technical FAQs

Ask a Question

What is the drop and pickup time for a 8501 RS relay?<br />

RS4 , RSD4 , RS14 , RSD14 RS24 , RSD24 pickup time is 25mS maximum and drop-out 25mS maximum .
RS34, RSD34 pickup time is 13mS maximum and drop-out 6mS maximum
RS41 , RSD41 , RS42 ,RSD42 , RS43 , RSD43 , RS44 , RSD44 pickup time is 20mS maximum and drop-out 20mS maximum .

20ms maximum.

CTA-ID : 2021402
Was this helpful?
What can we do to improve the information ?