Technical FAQs

Ask a Question

Will the 9001K4 fit the 9001KR1U operator?

Yes. Referred to page 17-83 in the Digest 173.
For the Type K non-illuminated push button standard. or mushroom. (9001KR4 and 9001KR5 mushroom buttons only.)


CTA-ID : 2020382
Was this helpful?
What can we do to improve the information ?