Technical FAQs

Ask a Question

What is the ATV31 cable that is used to connect to a PDA?

The pocket PC connection kit was VW3A8111.  It is now obsolete.
The kit consisted of:
* Two 0.6 m (2.0 ft) connection cables with two RJ45 connectors
* One RJ45/9-way SUB-D adapter for connecting ATV58 drives
* One converter marked RS-232/RS-485 PPC with one 9-way male SUB-D connector and one RJ45 connector
* One converter for ATV11 drives with one 4-way male connector and one RJ45 connector
It is necessary to have a cable kit for the handheld that allows for connection to a 9-pin parallel port. This should be available through the manufacturer of the handheld unit.

Reviewed 6/2011

CTA-ID : 2021370
Was this helpful?
What can we do to improve the information ?