Technical FAQs

Ask a Question

What is the wire size used to feed the factory installed QDL2200 disconnect installed in a QU12L400SL.

3/0 copper.


CTA-ID : 2021835
Was this helpful?
What can we do to improve the information ?