Technical FAQs

Ask a Question

Is there a NEMA 3R enclosure for field installation of the Class 8502 Type SDO* contactor?

Yes, use 9991SDH1 enclosure.

Note: Replace the reset mechanism with 9001K51 closing plate.


CTA-ID : 2021602
Was this helpful?
What can we do to improve the information ?