Technical FAQs

Ask a Question

What do we do on a I-line panel with 6 circuit rule and there is space for more than 6 breakers ?

Use one-way screw 21593-201-00 on the filler plates to prevent someone from adding breakers to unused space.

CTA-ID : 2022017
Was this helpful?
What can we do to improve the information ?