Technical FAQs

Ask a Question

The Ideal SureTest w/ AFCI fails to trip the Square D AFI breaker. Is the breaker bad?

Perhaps not.  There is only one true way to field test an AFCI and that is by using the test button on the AFCI itself.  The Ideal Sure Test units are UL listed as AFCI indicators (not testers).  AFCI indicators may not recognize all AFCI breakers, and should not be relied on to determine functionality of an AFCI circuit breaker.
The UL approved method of testing an AFCI circuit breaker is to press the push-to-test button when installed in an energized load center or panel.  This test injects a signal into the AFCIs sensor that looks like an arc to the AFCI.  A properly functioning AFCI will trip when the test button is pushed.  

Paragraph 31.8.1  of the UL 1436 standard requires the AFCI Indicator instructions to effectively state that the test button on the AFCI circuit breaker demonstrates proper operation.  


CTA-ID : 2022013
Was this helpful?
What can we do to improve the information ?