Technical FAQs

Ask a Question

Are the back panels of the HVL/cc Rear Extension removable? How many panels are there?

Issue:
Are the back panels of the HVL/cc Rear Extension removable?  How many panels are there?

Product Line:
HVLcc.

Environment:
Products sold in the United States.

Cause:
Assembly/ Installation.

Resolution:
Yes, the back panels of the HVL/cc Rear Extension are removable?
There is one panel for N1 indoor and three panels for N3R outdoor.


CTA-ID : 2021993
Was this helpful?
What can we do to improve the information ?