Technical FAQs

Ask a Question

QOMB3 will this accept a QO3 pole Circuit Breaker with a shunt trip

Yes this OEM Mounting Base will accept a QO 3 Pole Circuit Breaker with a shunt trip. Note that the breaker is wider than the base in this application.


CTA-ID : 2021792
Was this helpful?
What can we do to improve the information ?