Technical FAQs

Ask a Question

Can the side to side center floor channel of the indoor HVL switch enclosure be removed to avoid an existing conduit in the floor?

Issue:
Can the side to side center floor channel of the indoor HVL switch enclosure be removed to avoid an existing conduit in the floor?

Product Line:
HVL.

Environment:
Products sold in the United States.

Cause:
Assembly/ Installation.

Resolution:
Yes, the side to side center floor channel of the indoor HVL switch enclosure be removed to avoid an existing conduit in the floor. The enclosure must be securely anchored to the floor with anchor bolts at all four corners of the section.


CTA-ID : 2021996
Was this helpful?
What can we do to improve the information ?