Technical FAQs

Ask a Question

What type fuse is used for a AB1SF520M

5 x 20 mm. Unit is rated for 300 volts 10 amps per UL.
We offer the following fast acting fuses.
ABE7FU0500 = .5A
ABE7FU100 = 1.00 A
ABE7FU200 = 2.00 A
ABE7FU630 = 6.3 A


CTA-ID : 2021565
Was this helpful?
What can we do to improve the information ?