Technical FAQs

Ask a Question

What is the interrupting rating of the QO115 and QO120 breaker?

Prior to 1971 the QO interrupting rating was 5,000 amperes. In 1971, 10,000 amperes was optional and identified by a green handle. Starting in 1975, all QO115 and QO120 were 10,000 amperes, the green handle was eliminated and replace with a black handle.


CTA-ID : 2021561
Was this helpful?
What can we do to improve the information ?