Technical FAQs

Ask a Question

Does the ATS48 allow for an option for elapsed time meter?

Yes.
The open style unit already has the capability of displaying operating time in SUP menu. The parameter code is rnt and can be displayed in h or kh.
Additionally, the enclosed unit does have a modification of A08 which is for adding an elasped time meter to the enclosure.


CTA-ID : 2021261
Was this helpful?
What can we do to improve the information ?