Technical FAQs

Ask a Question

How far apart do you put the hangers on 4000 Amp, I Line II busway?

Issue:
How far apart do you put the hangers on 4000 Amp, I Line II busway?

Product Line:
Busway.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Indoor horizontal busway requires one hangar at least every 10 feet. Vertical Indoor busway requires one hanger at least every 16 feet. Outdoor Feeder Busway requires one hanger at least every 5 feet in either vertical or horizontal mounting. This information is printed on the nameplate of each busway device.


CTA-ID : 2021971
Was this helpful?
What can we do to improve the information ?