Technical FAQs

Ask a Question

What breakers were used in old style single phase UEZ Metering rated at 150 amps?

If the existing breaker is a Q2M2150MT use a QBM22150TN to replace it. If the existing breaker is a Q2M2150MB use a QBP22150TP to replace it.


CTA-ID : 2021741
Was this helpful?
What can we do to improve the information ?