Technical FAQs

Ask a Question

Was a 9007 Type B offered before the Type C ?<br /><br />

There was 9007B... Series of switches which were replaced by 9007C. There is also a 9007B head which is a current product for the 9007C line of switches.

Note that there is also Types 9007BD...which are European switches.



CTA-ID : 2021550
Was this helpful?
What can we do to improve the information ?