Technical FAQs

Ask a Question

Q1-100SL: What is the replacement?

QO2125SL is a 125A, 2 pole, plug-on sub feed lug kit, which can replace the older device which was rated 100A and required 4 pole spaces.


CTA-ID : 2021302
Was this helpful?
What can we do to improve the information ?