Technical FAQs

Ask a Question

Is there a way that the ATV58 can be shut down by an external fault?

Yes. The drive can be set up with any of 3 logic inputs programmed for external fault.
This ability became available as of 3rd quarter of 2002. For Altivar 58 drives up to the ATV58HD79N4 the control board must be revision V5.1 IE 32 or greater. For the larger drives, the revision must be V5.2 IE 09 or greater.
The parameter used in the setting for the desired logic input is Edd.

CTA-ID : 2020552
Was this helpful?
What can we do to improve the information ?