Technical FAQs

Ask a Question

What is the maximum back-fed main breaker ampacity that can be used in a HOM612L100RB load center?

The maximum back-fed main breaker ampacity that can be used in a HOM612L100RB is 100 ampere. Retaining Kit HOM1RK is also required for a back-feed application.


CTA-ID : 2021718
Was this helpful?
What can we do to improve the information ?