Technical FAQs

Ask a Question

What is the maximum branch breaker ampacity that can be used in a HOM612L100RB load center?

The maximum branch breaker ampacity that can be used in a HOM612L100RB is 70 ampere.


CTA-ID : 2021715
Was this helpful?
What can we do to improve the information ?