Technical FAQs

Ask a Question

How are the circuits numbered in a QO327M100 or QO327M100RB?

The circuits are numbered 1 to 30, with circuits 1, 3, and 5 occupied by a backfed main breaker. Odd numbered circuits are on the left, even numbered circuits are on the right.


CTA-ID : 2021954
Was this helpful?
What can we do to improve the information ?