Technical FAQs

Ask a Question

What is the part number for a Hand-Off-Auto control station for the Class 8911 Type DSG & Type DPSG NEMA 1 enclosed starters?

As outlined below:

For Compact 20, 25 & 30 amp Type DS*: Not available.
For Type DPS* 20 amp through 40 amp devices: 8911DSS1.
For Type DPS* 50 amp devices : 8911DSS1 & 9999BLX bracket.
For Type DPS* 60 amp through 90 amps devices: No kit available, suggest the use of 9001 Type K control station(s) mounted in the side of the enclosure.


CTA-ID : 2021240
Was this helpful?
What can we do to improve the information ?