Technical FAQs

Ask a Question

Can I order a shunt trip on the breaker in a plug-in unit such as a PFA32100G? How would I construct the catalog number?

Yes. Add the suffix of the shunt trip to the end of the busplug catalog number. For example, for a 120V shunt trip, the catalog number would be PFA32100G1021.

CTA-ID : 2021951
Was this helpful?
What can we do to improve the information ?