Technical FAQs

Ask a Question

What is the line voltage tolerance specification for the ATV11 unit?

ATV11....M2: 1-phase, 200 -15% to 240 +10%
ATV11....M3: 3-phase, 200 -15% to 230 +15%
ATV11....F1: 1-phase, 100 -15% to 120 +10%


CTA-ID : 2021157
Was this helpful?
What can we do to improve the information ?