Technical FAQs

Ask a Question

What is the AIR rating of the LC circuit breaker?

240 Vac rated at 100 kA
480 Vac rated at 65 kA
600 Vac rated at 35 kA


CTA-ID : 2022087
Was this helpful?
What can we do to improve the information ?