Technical FAQs

Ask a Question

What are the ``K`` ratings for an F-frame Powerpact breaker, like the FKA160151?

120V 100kA
277V 65kA
347V 65kA


CTA-ID : 2022077
Was this helpful?
What can we do to improve the information ?