Technical FAQs

Ask a Question

Can a HDF/HGF/HJF/HLF or JDF/JGF/JJF/JLF frame breaker be reverse connected !?

No , these frames with field installable trip units have line and load markings and are not suitable for reverse connection.


CTA-ID : 2021943
Was this helpful?
What can we do to improve the information ?