Technical FAQs

Ask a Question

Can 100% rated breakers be used or obtained with the EZM Main devices or EZM branch devices?

Issue:
Product Design

Product Line:
EZM Metering

Environment:
Main Breakers

Cause:
Application

Resloution:
No. The EZM Main Devices or branch devices are NOT rated for use with 100% rated breakers. They use 80% rated breakers only.

More info on EZM Metering here.
 
Was this helpful?
What can we do to improve the information ?