Technical FAQs

Ask a Question

What is the mean time between failure for the ATV31 (MTBF)?

The Average is calculated on the ranges 200V & 500V ATV31 M2/M3X/N4:
=> MTBF = 120000H
** This figure is as of September 2004 and may be updated over time as real time experience affects the MTBF numbers. **


CTA-ID : 2020443
Was this helpful?
What can we do to improve the information ?